This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC256404: 關於LLC的諧振電感,諧振電容,以及變壓器的漏感

Part Number: UCC256404
Other Parts Discussed in Thread: PFCLLCSREVM034

各位先進大家好:

我買了一塊PFC+LLC的發展板,PFCLLCSREVM034,但是在設計上,關於諧振電容、諧振電感,以及變壓器的漏感,我有些疑問:

1) 我從datasheet的設計範例以及設計工具UCC25640x Design Calculator Rev4.0 可以知道,諧振電容的值為0.03uF = 30nF,

    但是我在電路上找不到這個電容,也許這個電容是幾個不同的電容串聯並聯組成的?不知道能不能指給我看一下?

2) 在這塊發展板的使用者手冊上,並沒有提供變壓器的詳細規格。只有在電路圖上寫了Lm=510uH 以及圈數比為 33:3:2:2,並沒有提到變壓器的漏感大小。至這個問題跟我的下一個問題有關

3) 當我們設計出諧振電感以後,可以獲得電感值,那麼這個值需不需要考慮到變壓器的漏感呢?比方說,如果設計出來諧振電感為100uH,而變壓器的漏感為30uH,

     那麼,我應該使用100uH的電感,或是使用100-30=70uH的電感呢?

麻煩有經驗的先進可以給我一些寶貴的建議。謝謝