Other Parts Discussed in Thread: TPS54260,
1、TLV62569DBVR作为二级电源输出3V使用,一级电源为TPS54260输出5V电压,供电范围为9——36V。
2、TLV62569DBVR原理如下所示
3、设备出现所有问题都是TLV62569DBVR,一级电源没有损坏,用电端没有出现损坏,更换TLV62569DBVR后可以正常使用,所有损坏TLV62569DBVR表现为SW对地短路。芯片损坏一般在设备投入使用2个月后开始损坏。
4、设备销售至今共返修15台,并随着销售量增加,返修也在增多。
5、所有设备出货前全检没有问题,出现问题都在客户使用一段时间后出现损坏。客户通常在机柜使用,电源供电采用12V/24V开关电源。
6、在出现问题后我们对设备供电进行破坏性浪涌、脉冲群测试(5000V)未出现损坏。
需求如下:
1、请帮忙分析芯片损坏原因?
2、对于目前我们使用电路是否能够进行优化避免损坏?