设计中使用的是内部温度采集,BQ34Z100有3个区间,每个区间对应一个充电电压,-10~10,10~45,45~55,如果检测到的温度超过了55V,这时候BQ34Z100内部的一些寄存器为0,比如表示充电电压和充电电流的寄存器,(电压)0X30/0X31。
1.请问这种条件下对电量有什么影响呢?
2.如果将FC SET%=-1,上述条件下,是不是永远无法满足FC条件呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
设计中使用的是内部温度采集,BQ34Z100有3个区间,每个区间对应一个充电电压,-10~10,10~45,45~55,如果检测到的温度超过了55V,这时候BQ34Z100内部的一些寄存器为0,比如表示充电电压和充电电流的寄存器,(电压)0X30/0X31。
1.请问这种条件下对电量有什么影响呢?
2.如果将FC SET%=-1,上述条件下,是不是永远无法满足FC条件呢?
1.温度对电量影响表现在guage内部的阻抗跟踪算法上,一般来说温度高电池内阻小,温度低内阻变大,内阻大了 剩余容量也就小了,这种现象在低于15度时会比较明显。你说的这几个寄存器和这个的关联不大
2.这种情况属于过温,建议不要进行充电,不充电自然也就无法满足FC 条件,当然如果你在没有FET过温保护电路强行充,那也是可以充的到FC置位的