This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM41625-2X-EVM: 电源评估板

Part Number: TPSM41625-2X-EVM


在使用TPSM41625-2X-EVM评估板时,遇到输出电流上不去的问题,手册并未提及限流的相关问题。测试情况如下:

Vin = 5V,Vout = 0.9V。

1、当输出电流10A时,TPSM41625-2X-EVM电流输出只能到9.5A左右;

2、当输出电流大于10A时,TPSM41625-2X-EVM电流输出也只能到9.5A;

请问发生这样的情况时什么原因造成的?

备注:

测试Vin = 5V,Vout = 1.8V。TPSM41625-2X-EVM电流输出可以大于10A,但到19A左右就上不去了。