This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3525A: PWM控制IC选取咨询

Part Number: UC3525A


目前需求是这样:

外部的电压电流环路是自己用运放搭出来的,然后将电流环的输出送到PWM 控制器中

PWM的控制器可以设置锯齿波频率,最好能到1M, 生成两路互补驱动波形(最好带死区),驱动高电平能大于7V

最大占空比最好能达到100%(看了很多PWM IC最大占空比只到50%,理论基础不够,不太明白原因)

此外还有个问题请教一下,为什么PWM IC内部生成的锯齿波最低电平在1V而不是0V,麻烦不吝赐教,有没有TI出的关于PWM IC的pdf可以学习一下

谢谢