hi:
客户在调试新的项目时,有一部分LM36011 显示Flags Register (0x05) LED Short Fault。
1. LED PIN 上的电压确实不足 0.5V.
2.断开LED PIN上LED.
3.强制软件复位,Register0x06 bit [7]), Flags Register (0x05) LED Short Fault 会复位为0,过一会也是会显示1.
芯片太小,客户没有办法做ABA交叉验证
想了解,能判断出芯片是坏了嘛?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi:
客户在调试新的项目时,有一部分LM36011 显示Flags Register (0x05) LED Short Fault。
1. LED PIN 上的电压确实不足 0.5V.
2.断开LED PIN上LED.
3.强制软件复位,Register0x06 bit [7]), Flags Register (0x05) LED Short Fault 会复位为0,过一会也是会显示1.
芯片太小,客户没有办法做ABA交叉验证
想了解,能判断出芯片是坏了嘛?
Hi
要么确认LED, 要么确认芯片, 如果不想更换芯片确认,建议更换LED确认(用热风枪更换,无论是LED,还是芯片,更换是很容易的)
Johnsin:
客户有直接更换LM36011,问题就解决了,针对这个Flags Register (0x05) LED Short Fault报错的现象,还有什么建议嘛?
Hi
更换好芯片后就不应该有这个异常,因为之前输出0.5V导致检测到异常。
hi Johnsin:
我确认一下,如果更换LM36011能解决问题,那芯片发生了问题。