This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS562202: TPS562202

Part Number: TPS562202


想问一下,有没有专家知道在tps562202搭的降压电路中(12V转5V),测试时输出电压出现纹波噪声大的情况,并且输入电压也会和输出电压一样出现大的噪声,如下图

添加负载测试时,噪声情况更严重(输入为12V,测试出来是5~30V)

想问一下有没有好的解决办法

  • Hi

        输入输出的纹波noise都很大,受限要确认是否受到外部干扰(比方说靠近电源芯片又电机之类的干扰源)

        其次确认一下GND的布局(建议参考datasheet)。

  • 感谢您的耐心回答,还有一个问题是,在加入负载进行测试时,测量输出电压,发现电压均值相比于空载测量时,上升了0.5~0.6V,不知道这是由于什么样的原因造成的?

  • Hi

        一般来做,重载时输出电压会比较空载时电压略微低一点点(0.1V左右可能时正常的), 而你的测试相反,并且差异很大,很可能是反馈受到noise影响或者是layout等导致输出稳定引起(这种影响在小电流时影响较小,而电流较大的影响显现出来)