你好,
我看了一下TPS54202 datasheet,里面只是说为了提高轻载的效率,建议取值从100KΩ开始。针对TPS54202的R2和R3的取值,我这边打算用到40.2KΩ+6.8KΩ这样的搭配,请问有没有绝对不能用多少KΩ以下的电阻呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
我看了一下TPS54202 datasheet,里面只是说为了提高轻载的效率,建议取值从100KΩ开始。针对TPS54202的R2和R3的取值,我这边打算用到40.2KΩ+6.8KΩ这样的搭配,请问有没有绝对不能用多少KΩ以下的电阻呢?
HI
可以的,主要是建议高边电阻为100kohm,可以小于,但不能大于100kohm, 所以你选择40.2kohm+6.8kohm是可以的。
只是相对100kohm+16.9kohm,反馈电阻消耗的功率略微大一点点,但是也不会很明显,不过你可以略微将电阻再放大一点点。