Part Number: TPS7B84-Q1
我看此类芯片目前都处于缺货状态,目前的应用场景是输入24V,可能max要达到30V,输出是7V主要,电流要求100ma,要求噪声较小,用在模拟采集应用中,是否有芯片可以推荐的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS7B84-Q1
我看此类芯片目前都处于缺货状态,目前的应用场景是输入24V,可能max要达到30V,输出是7V主要,电流要求100ma,要求噪声较小,用在模拟采集应用中,是否有芯片可以推荐的?
Hi
中设置一下输出输入电压大于25V, 输出电流建议大于300mA(因为输入输出压差比较大,建议至少选择300mA以上),并输出可调,剩下的芯片就不是特别多了,然后你可以联系购买渠道再确认。(你还可以根据你的需求再额外增加条件,例如价格之类)
不过建议你采用DC/DC+LDO的方式来做, 因为输入输出压差太大,假设你输入30V,输出7V/100mA, 效率只有23%左右,芯片功耗2.3W, 会造成芯片严重的温升,散热上需要特别注意(需要根据热阻信息选择散热方式)