This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25141-Q1: DLP5530中的LM25141损坏问题

Part Number: LM25141-Q1
Other Parts Discussed in Thread: LM25141

DLP5530EVM,在使用的时候,一开始是OK的,后突然出现画面闪一会然后就不亮了,RGB等都没亮,重启多次没改变,后检查发现LM25141的HB引脚是短路的,然后测试FB脚、VDDA脚、VCC脚都是没有电压的,就是DLP5530EVM的LED驱动板上面的那颗LM25141,估计是HB未知什么原因与地短路了,导致VCC过流内部LDO损坏,故没了VDDA和FB电压VREF,最后SW等引脚都是0V,BUCK有12V的输出却没有输出8V或者6.5V,请问什么情况会HB损坏?静电?没有碰它

x 出现错误。请重试或与管理员联系。