Other Parts Discussed in Thread: BQ25170
您好,
请问bq21040 规格书充电电流支持10mA,但是推荐使用时只推荐充电电流在50mA,请问如果使用10mA充电电流,会有什么影响吗?或者,怎么可以避免影响呢?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
从参数表(Page5)看充电电流为10~800mA.(其他描述确实是50mA~800mA), 但是充电电流一般不会设置到很小,因为这个会严重影响充电时间,例如本身设置800mA充电,改为充电10mA, 充电时间可能至少充电长80倍(假设本身1小时能充满结果要充电80小时才行,这个是很没有必要的)。