This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61500遇到的问题

Other Parts Discussed in Thread: TPS61500

最近在做一个案子,输入:单节锂电池(工作电压范围:3.0-4.2V),输出:48颗直径5MM双晶片紫光LED(VF=3.2V,IF=40mA),采用4串12并的链接方式,即总电压为12.8V,总电流为480mA。采用TPS61500驱动,发现只有当输入电压大于5.0V时LED电流才能恒定在480mA,而在3.0-4.2V的电压范围内时,随着电压的减小,LED电流也在减小,并且最大时也达不到480mA,感觉此时恒流已不起作用。卧式按照TPS61500规格书上的电路连接调试的,其中L1=10uH,D1=SS14,C4=470nF,C3=C5=0.1uF,R4=200K,C2=22uF/25V

哪位高手能帮忙分析一下,不胜感激!