This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40305: TPS40305产生的电压被负载拉低

Part Number: TPS40305


TI的老师:

您好。

我的一个设计采用了 创龙的6678核心板,该核心板需要外界9V供电。我在底板上做了一个基于TPS40305DRCR的12V转9V电压转换电路,然后把TPS40305产生的9V电压提供给6678核心板,TPS40305DRCR的电路是利用webench生成的,9V/3A输出。

我现在遇到的问题是,在不挂载核心板的情况下,测量TPS40305产生的电压是正常的。但是一旦挂载核心板,TPS40305产生的电压会被拉低到4.3V左右,Pgood也被拉低。一开始我以为是6678核心板的外围电路设计哪里短路了,直到我测试了一种情况:飞两根线:(1)共地,(2)底板产生的9V飞线直接供给6678核心板。仍存在9V电压被拉低的情况。但是这个时候如果我稍微拨动一下那根飞出去的地线(这根地线焊接的不太牢固),9V电压就恢复正常了。我用稳压源直接给核心板供电,核心板工作正常,上电工作电流不到1A,低于TPS40305DRCR能满足的3A输出。我还尝试了一下把TPS40305DRCR外围的那个电感拆掉(图1中的L1),两个焊盘直接用锡连起来,这个时候即使不挂载核心板,TPS40305产生的电压也在4.3V左右了。这个现象我也不太理解,电感也会影响输出电压么?而不是仅仅滤波的作用?

恳请TI的老师帮忙分析一下原因,谢谢!