This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610: 充电问题

Part Number: BQ24610

设计参照 bq24610使用手册Figure 20. System Schematic with Power Path

供电电压ADAPTER 为28V,PACK为7.4V   2节串联锂电池

V(BAT)+7.4V     I(DPM) 设置为4A    I(PRECHARGE)设置为0.3A     I(CHARGE)设置为2.5A

TTC下拉一个0.1uF电容

TS接了一个插件式10K NTC热敏电阻接电池负极绑在电池上的

通电后测试数据VREF,CE正常,ACSET,ISET2,ISET1 电压与我设置的值相近

问题:

1.未接通锂电池STAT1 状态指示灯亮,PG指示灯不停闪烁

2.接通电池后,供电用的直流电源为0.1A左右,电池接口电流为0.221A,电压7.6V左右,因为接了一个直流电压电流的LED显示器数据还算正常

但是充电半小时后供电电源电流突变为0.02A左右与未接电池时相似,电池接口的电流直接为0