This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54202: EN引脚问题

Part Number: TPS54202


如上图所示,R5本来需要贴105K,而贴成了1M,如果不考虑使用其中的调节欠压功能的话,这样会对芯片稳定或者性能造成影响吗?

目前我们有贴了5000多套,但是测试没有什么问题,输入电压24V,EN引脚按阻值分压应该是16V,实际测试接近7V。

看了规格书,EN引脚是0-7V之间,是内部钳位住了吗?这样长期使用会不会有什么影响?

  • HI

       需要将电阻改过来,不能用成1Mohm,芯片内部没有钳压设计,只有上拉电压源。

       EN只有7V,将分压电阻拿掉, 测试EN脚拉低到0V是否能关闭芯片? 重新给3.3V能够启动芯片。这样是为了判定芯片EN脚是否已经损坏?

       但是无论是否能正常工作?或者芯片是否损坏,不能用1Mohm电阻,如你所说,分压达到16V是有问题的,即便芯片仍能正常工作。

       将电阻改回来并不麻烦,用热风枪更换。