This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5175: 输出纹波形状和幅度在输入电压为12.3V~15V区间异常变大,有时候电感啸叫

Part Number: LM5175

Hi,TI的各位专家:

  你们好,我的设计是用LM5175适配9~24V输入,产生额定6A@12V恒压输出,用的是WEBBENCH的电路,电感是3.3uH。效率测试基本都符合预期,较高的。

  补充说明:

    纹波测试方法:通过两根很粗的导线(导线长度8厘米)把输出引到66uF陶瓷电容上,然后再用60厘米的导线从电容连接到电子负载,纹波+噪声测试点在所述66uF的电容上。

    纹波:此处所述纹波是指示波器全带宽条件下测得的纹波+噪声。

存在的问题:

一:设置负载电流为1A,测得输出纹波形状和幅度随在输入电压为12.3V~15V区间异常变大,分别如下图1~图3所示,其中VIN=14.9V时,输出纹波那种尖峰出现的频率比VIN=15时明显增多,且此时电感出现轻微啸叫,若此时降低负载电流至0.8A以下,则输出纹波波形和幅度则类似图4所示,且电感啸叫消失。

二:其他输入电压区间,输出纹波和噪声波形基本类似如下图4所示,正弦部分的整体幅度是比较小的。

三:上述现象是正常的吗?若不是,应如何解决。

  

           图1 VIN=15V时的纹波波形                                                                    图1 VIN=15V时的纹波波形ZOOM IN

                   图2 VIN=14.9V时的纹波波形   

  

                图3 VIN=13.6V时的纹波波形  

                  图4 VIN=12V时的纹波波形