我们采用BQ24600设计4节锂电池(单节电压3.7V-4.2V)充电管理,参考芯片datasheet种推荐的原理图做了对应需求参数调整。设计指标电源输入24V、5A,电源输出16.8V、6A(用于4S电池充电)。实验结果为能对4S锂电池进行充电,不过功率较低,输入端24V、0.6V,输出端0.8A,与预计设计功率不吻合。请大神帮忙看看问题出现在哪里?
(1)上管MOS栅极波形
(2)下管MOS的栅极波形
(3)经过电感前波形
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.