This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61022: 使用过程中出现莫名烧坏

Part Number: TPS61022


问题描述:1.在调试时,输入电压为3.8V,输出电压5V, 在经过一个MOS 管给一个4G模块供电。

当把MOS管打开给4G模块供电时(4G模块5V,瞬间电流3A),TPS61022就烧掉,瞬间有青烟冒出。

 

 

 2.更改TPS61022的工作模式,把6脚接成高电平,此时按手册说明为强制PWM模式,

输入电压3.8V左右,输出电压5V, 且不给打开后级电路,即5V 不给4G模块供电,理解为无负载,不做任何操作,该芯片输入端电流能到达50mA,3-5秒钟后,输入端电流达到2A;停止供电,测量7脚对地已经短路了。

 

3.更改5脚分压电阻,R113=300K,R116=100K,网络标号5V-EN电压为3.3V,那么5脚电压分压后得到0.8V,芯片无法打开工作,芯片发烫,且无法输出5V 电压。

VEN_H这个脚上的电压阈值是多少?大于多少伏此芯片可以工作?

针对调试过程中出现的以上3种情况,烦请分析,告知原因。