This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350: BQSTUDIO 连接问题

Part Number: BQ78350
Other Parts Discussed in Thread: BQSTUDIO,

您好:

1、我们这边打板有的板子用BQSTUDIO连接BQ78350 用smbus方式连接没有任何反应,其中有块板可以正常连接BQstudio,也烧录了官网的固件bq78350_R1_v1_04_build_26.srec,而且也正确配置了4节电池,使能了FET_EN,可以有电压输出。然后过了几天再次连接bqstudio,smbus方式一直连接不上,想问下有哪些原因造成连接不上。与bqstudio 软件启动选择会有个Target Selection Wizard里的Please select a target....中选错芯片的版本型号有关系吗?(比如其中里面有1E9B_1_03-bq78350_R1.bqz、1E9B_1_04-bq78350_R1.bqz、1E9B_2_02-bq78350R2.bqz这些),假如这个地方选错导致后面连接不上,哪有什么办法重新正常连接bqstudio,再次重新烧录固件呢?

    2、由BQ78350DBTR-R1换成BQ78350DBTR-R1A对于bqstudio连接是否有影响,另外再bqstudio 启动选择型号,应该选择哪种(比如其中里面有1E9B_1_03-bq78350_R1.bqz、1E9B_1_04-bq78350_R1.bqz、1E9B_2_02-bq78350R2.bqz这些)

   3、BQSTUDIO连接BQ78350 的sumbus地址显示为0x17,看spec里面地址为0x16或者0x17。不能正常连接bqstudio是否需要配置哪个地方,具体如何设置