This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62569: 低温(-25℃)运行发生芯片短路故障

Part Number: TLV62569


产品出厂测试都会测试电源芯片TLV62569输出电压以及断电情况下的对地电阻,均正常,而且产品出厂时需要做12小时的老化运行测试;

此故障是在现场应用产品上面发现的,进入12月份以来发现应用在黑龙江、吉林和辽宁省的产品陆续出现返修(产品使用环境温度 -25℃),返修故障均集中在相同的位置,都是ARM核心供电的5V1VTLV62569无输出电压,系统无法启动; 故障芯片 VIN管脚(5V)与SW管脚(1V),SW管脚(1V)与GND管脚电阻非常小,接近0;详见下图。

Pin to GND

Broken chip

Normal chip#1

Normal chip#2

Normal chip #3

VIN-GND

 0.3R

 ∞

 ∞

 ∞

SW-GND

 0.3R

 ∞

 ∞

 ∞

FB-GND

 31M

 ∞

 ∞

 ∞

EN-GND

 ∞

 ∞

 ∞

 ∞

相关原理图:

另外:

同时作为对比,该产品有两套BOM,使用钰泰ETA3485的批次到目前为止一片都没有出过类似故障,两者的差别是ETA3485是定PWM控制,而TLV62569是变PWM的,请分析是否和这有关系;