This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL7660: 关于该芯片的一些疑问

Part Number: TL7660
Other Parts Discussed in Thread: TPS63710, LM27761, LM2776

工程师您好,

最近正在考虑使用TL7660,通过将+5V转化为-5V,给运放供负压电源。

问题如下:

1.请问7660在-5V输出情况下,输出电流最大可以到多少?如何评估输出电流?

2.在规格书第8页结尾处,建议输入大于3.5V时,LV不能直接接地,请问此时悬空是否可以?

3.接问题2,我在规格书中看到,OSC和LV管脚是控制内部RC转换器的,请问这俩管脚在实际应用中起什么作用?该怎么应用?

4.电荷泵反向稳压器(例如TL7660),与带内部转换器的反向稳压器(例如TPS63710),有什么区别?选型的时候该如何考虑?

  • Hi

       1. 输入5V,输出电压和负载电流可以见datasheet 第5页最后一个图,可以看到最大40mA输出,并且电流越大,输出负压偏离-5V越大,所以如果要越接近-5V,建议负载不能太大。

       2. 输入1.5V~3.5V,  LV接GND.   输入3~10V,  LV悬空。 所以如果你输入大于3.5V,  LV是需要悬空的。

       3.  LV配置如上,OSC是频率设置,见datasheet第4页第一个图。

       4.  TL7660是电荷泵,电路简单,但是负载能力差,同时随负载加大,输出电压偏离反向电压越大。TPS63710是电源转换器,电路相对麻烦(需要磁性元器件电感),带载能力强。输出电压精度较高,不会随负载加大输出电压出现偏离。

  • Hi   

        TL7660输出电压准度相对较差(输出偏离较大),可以选择其他一些电荷泵,有一些输出偏离相对较小的。

  • 请问是否有其他型号推荐?

  • HI

        如果你需要比较准确的-5V, 你可以选择带有LDO的chargepump, 例如LM27761之类,还有个好处就是纹波非常小,因为是LDO输出。

        如果不需要太准确,可以选择LM2776之类,5V输入大约-4.85V左右输出。

        这类芯片比较多,你可以看看: www.ti.com.cn/.../products.html