This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5175: 输入18V输出28V空载时电压异常最高达到30V

Part Number: LM5175


Dear TI:

              设计输入18-36V输出28V,当输入电压低接近18V空载时输出电压异常纹波达到2V最高电压30V。

               输入电压抬高,输出电压正常。

               输出增加轻负载(100mA),输出电压正常。

               MODE改为CCM模式,输出电压正常。

               测量异常的时候SW输出频率非常低,COMP电压为0V。

               跟参考设计的区别是:MODE设置为DCM,参考设计为CCM,设置为DCM模式的原因为可以降低静态电流。

               请TI协助解决,谢谢~~~