This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM5601R5: 关于芯片AGND与PGND的一些疑问

Part Number: TPSM5601R5

工程师好,

最近在看该电源模块,目标是将12V转换为3.3V,有几个问题需要咨询下:

1.规格书第3页对于AGND的描述中,说AGND必须与PGND单点相连,用0欧电阻进行单点接地是否可以?

2.接上问题,如果AGND与PGND直接相连,会存在什么问题?

3.规格书第3页,当PGOOD不用时,可以悬空,如果PGOOD悬空后,V5V管脚是否也需要直接悬空?

4.规格书第3页,对于SW的描述,实际应用中应该是直接悬空的,既然如此,为什么不直接把该管教命名为DNC呢?

多谢回复!