This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54561: 关于软启动的疑问

Part Number: TPS54561

上图为电源芯片手册软启动部分描述

电容的定义为每升高1V需要的电荷量,即C = Q / V

电流定义为单位时间内流过导体横截面的电荷量,即I = Q / t = C * V / t

高亮部分的电容量为87uF,升压值为5V,以此充电平均电流为1A,以此计算,充电时间为t = 5 * 0.000087 / 1 = 0.000435 = 0.435mS

问题1. 以上计算是否正确呢?该部分的0.3mS是怎么计算出来的呢?

问题2.对于不同负载条件,应该如何考虑平均软启动电流Issavg呢?我在数据手册中没有找到,设置为多少相对安全呢?