This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMG1210: 驱动GaN或者NMOS高端输出不正常

Part Number: LMG1210

想用LMG1210和氮化镓做一个半桥电路,但是目前测试发现输出高电平只有4.6V

原理图如下

19脚(PWMA)拉低,LO输出4.5V,HO输出0V,OUTA的电压为0V是正常的。17脚(BST)电压为5V,12脚(HB)电压为4.9V。

但是PWMA拉高后,LO输出0V,HO输出4.5V,OUTA的电压只有4.5V左右,这时候测量HS的电压也为4.5V左右。17脚(BST)电压为5V,12脚(HB)电压为4.8V。

开始怀疑是GaN的问题,后来换成NMOS,现象一样。