This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90120A: 响应延迟

Part Number: UCD90120A

我们发现同一个PLD而且同一个FW,但每次上电的时间不太一样。请问这是什么造成的?

请参考下面两个图,这两个图是在同一个板子用同一个FW产生的不同上电时间(9ms和150ms)。

说明:3.3V_PCIE是PLD的POWER,RESET是PLD的复位信号,P12V_PGD_VR是一个input信号,P1V8_EN是检测到P12V_PGD_VR为高时,输出为高。Delay=0ms*P12V_PGD_VR(Active High)

另外,当出现上电时间比较长的时候,经过检查PLD的设置,发现有错误。