Part Number: LP55231
一个IC控制9个LED,RGB的5050封装,然后使能开启,
ENABLE_CHIP =0x41
OUTPUT_ON1=01
OUTPUT_ON2=FF
MISC = 51
VARIABLE=FF
可以点亮,但是电流太小,在PWM和电流都设置成最大的情况下,输出电流也就只有8mA(G和B)而红色只有5mA,
请问是寄存器设置的有问题吗?如何解决; VDD=5V , D1,D3,D5是绿色,D2,D4,D6是蓝色,D7,D8,D9是红色
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LP55231
一个IC控制9个LED,RGB的5050封装,然后使能开启,
ENABLE_CHIP =0x41
OUTPUT_ON1=01
OUTPUT_ON2=FF
MISC = 51
VARIABLE=FF
可以点亮,但是电流太小,在PWM和电流都设置成最大的情况下,输出电流也就只有8mA(G和B)而红色只有5mA,
请问是寄存器设置的有问题吗?如何解决; VDD=5V , D1,D3,D5是绿色,D2,D4,D6是蓝色,D7,D8,D9是红色
HI
这个芯片电流是通过内部设置,如果确认LED电压没有问题,很可能就是数据没有写进去。
Hi
将电路贴上来看看,另外有没有做一些电压测量?