设计采用TPS650864给ZYNQMP供电,其中,PL的VCCO为SWA1供电,设计电压3.3V。调试时,连续两块板子使用一段时间后出现PL的HDIO损坏,始终为高。示波器测量为3.3V,纹波偶尔超过3.4V,时间不超过10us。看ZYNQMP手册发现VCCO最大耐压为3.4V,请问设计是否有问题?


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
没有问题的。不过一般芯片的供电为3.3V的话,最大电压不会只3.4V这么小?
另外确认一下纹波,不应该超过30mV.