This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3409HV: LM3409HV demo 设计 Q3管子烧毁

Part Number: LM3409HV
Other Parts Discussed in Thread: LM3409

您好:

1、我们现在在用LM3409HV这款芯片,像要实现如下需求:
输入电压:36V
最大输出电压:25V
最大输出电流:>2A (电流大小可调节)
频闪调光速率:>100K 

2.根据这款芯片的DEMO,做了一个样板,但是没有实现PWM调光,DEMO如下

3.问题:通过外部PWM调节,Q3管子会烧;也试过用EN管脚进行PWM调节,但是用EN调节电流上升很缓慢,上升时间达到了3uS以上,下降时间也很缓慢,如果能解决上升和下降时间缓慢问题,EN方式调节也是可行的

上图黄色波形是电流,绿色是外部pwm,目前设计的样板就是按照如下该图设计的,麻烦帮忙给以分析或者优化设计,十分感谢