Part Number: LM5176-Q1
Other Parts Discussed in Thread: LM5176, TPS40057
TI工程师你好!
目前计划使用LM5176-Q1设计电路。对于LM5176的功耗计算这里不知道要如何计算。5176使用外部桥臂驱动MOS管,其功耗主要是内部逻辑电路和驱动场管的电路损耗。具体要如何计算?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
Datasheet 第25~26页有计算MOS的功耗,另外就是芯片的静态功耗(输入乘以静态电流),以及电感的功耗(DCR的功耗)。
整体计算比较麻烦,但你可以借助webench在线仿真来计算。
感谢陶工的答复!
芯片的功耗应该包括逻辑电路的功耗和驱动电路的功耗。逻辑电路输入电压是VIN或者VBIAS电压,而电流按照下表的那个值来算?是4mA还是64mA?

驱动电路部分是按照下表的电流和电阻来算?

就是芯片的功耗如何同真个电路的输出功率挂上关系?我现在需要计算芯片的功耗,然后设计散热方案。目前电路方案是输入8~36V输出12V/12A
Hi
是4mA, 64mA会在驱动功耗中体现出来。
陶工你好!
内部逻辑电路功耗我按照P=VIN*4来算,那芯片驱动部分的功耗要如何计算吗?就是下图一的红框部分,和下图2的红框部分有关系?


Hi
这款芯片datasheet上的计算并不全面,你可以参考一下TPS40057等同步buck芯片MOS, 驱动功耗的计算。但是LM5176相对复杂一些,因为它是buck-boost架构。
HI!
我在官网上对LM5176进行电路设计,它给出的芯片功耗可以作为实际使用的依据?因为我使用的功率较大,而参考设计貌似无法进行两个场管的并联使用设计。直接输入输入8~36V输出12V/14A会提示错误,但是先输入6A进入设计页面再修改成14A又可以。

Hi
webench仿真的数据是可以作为参考的。
但如你所说,这个软件也有不灵活的地方,例如如果你想MOS并联,但是并不能通过软件来设置。
HI!陶工!
我看了TPS40057同步buck芯片MOS,驱动功耗的计算,有点疑问请教一下。如下图所示。公式41计算的是单管驱动电路的功耗,公式42是计算上下管相同的时候2个管子的驱动功耗。公式41如何推导到公式42?为什么在计算内部逻辑功耗的时候使用的是VIN而不是VIN-内部稳压器输出电压?谢谢!