Other Parts Discussed in Thread: BQ25170, BQ25180
我们的蓝牙小系统,充电电流也就75mA左右,请问下,BQ25175和BQ2510X这两颗料哪款是主推物料呢?
另外问下BQ25175是否可以用于4.2V的电池充电?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,对于 75mA 充电电流和 4.2V 电池电压来说,BQ25170 或 BQ25180都可以。
BQ25175 的电池稳压电压为 4.35V。