Part Number: TPS61196
VIN:12V
VOUT:36V
ISET:80mA
fsw:200KHZ
PWM:频率f:2khz;占空比D:0.06%
当PWM占空比由10%调至0.06%时,常温下(25℃)LED可正常工作,但在高温下(70℃),LED不工作,并且讲占空比调回10%时,LED也不工作。
想问:PWM的占空比(或PWM开启时间)受哪些因素影响?内置MOS管的爬坡时间?SW的PWM控制模式和PFM控制模式的转换时间?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
如果调光工作频率是200Hz, 占空比0.06%,或者0.1%测试一下是否仍有问题? 如你所说,频率太高,太短的时间可能有问题。