Other Parts Discussed in Thread: LM5117
初次应用LM5117,需要请教几个问题:
1:12v输出,当负载大于1A时,VIN的3.9 OHM限流电阻发热严重,直到烧毁,请问会是什么原因
2:需要做12V/20A输出,有哪些地方需要特别注意的?
希望有经验的同行指教。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
电阻封装是否0805? Vin的电流并不大,除非异常电流导致电阻功耗特别大, 注意建议选择的MOS Qg尽量小一点,并且Vin的电容尽量靠近Vin脚。
特别注意的地方主要是layout, 因为电流比较大,如果layout不好寄生参数容易造成电路不稳定,设置带载能力下降。
HI
按照参考设计的0805封装即可。这里电流并不大。