This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3430-Q1: 关于TPS3430的 CWD和CRST管脚的疑问

Part Number: TPS3430-Q1


1.CWD引脚:可以通过CWD不同的管脚配置,来改变看门狗输出的高脉冲和低脉冲时间?如CWD = NC, SET0 = 1, SET1 = 1  低电平持续时间800ms(type),低电平持续时间1600ms(type);不同的配置只是更改高低电平的时间吗?是这样的吗?

2.CRST管脚:通过不同的配置,实现实现看门狗输出延迟时间?如CRST NC时,看门狗输出延迟200ms(type);是延迟200ms后,根据CWD的引脚配置的高低电平时间,WDO输出相应的脉冲?

3.CRST脚接地会怎样?按照TI文档提出snva837.pdf 文档提出WDO的锁存;当输出WDO低电平时,通过缓冲器将CRST拉低,此时WDO输出一直为低,实现了锁存,是这样的吗?在规格书中并未给出CRST接地,芯片会怎样,麻烦TI相关工程师,帮忙解答下,谢谢!