This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3150: 输出纹波大,达到正负2.5V。

Part Number: LM3150

Hi, 你好 ,我的需求是设计制做一个DC24V转DC12V的电源,Iout-max=10A ,Iout 通常工作为5A , 纹波要求控制在50mV以内 , 输出电压范围为DC12V+-5%  ,  参考WEBENCH推荐电路,在实践测试后对Ron、Rlim及Css进行测试修改后,以如下电路在工作。电路的输出带载能力符合预期。

问题:对输出端使用示波器测量其交流分量 ,可以看有正负5V的脉冲,脉冲频率与LM3150芯片HG端频率一样,下图是在输出端的交流分量图,请教该怎样减小输出纹波,达到目标<50mV以内。