Part Number: TPS5430
Other Parts Discussed in Thread: LM22676


请问,使用TPS5430,输入电源24V,输出-15V,实际电流只有几百mA,但在实际应用中,会偶现电压无输出,是否是因为24-(-15)=39V,超出最大输入36V限制???导致芯片工作异常。如果是这个问题,有没有其他替代料?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
对的,输入电压已经超过设计规格,按照你的需求是需要选择输入大于39V的降压芯片,你可以选择如下:
如上降压芯片(内置MOS)List, 设置一下最大输入电压大于39V小于60V, 输出电流大于3A小于5A, (或者你可以略微调整下),会发现仍然有非常多的芯片适合你的设计,
然后再结合成本,设计难易度(可以选择不要外部补偿同步MOS的降压芯片)等进一步筛选。
Hi
电流足够是可以的,因为这个芯片是42V最大输入。