Part Number: UCC27614
需要选用一款PWM控制器配合C2000控制器给pmos供电。
要求:输出电压在0.12-0.3 V间可调,调节精度为0.01 mV。
请问UCC27614能满足上述要求吗?如果不能,可以推荐几款吗?
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
直接用C2000的I/O口加驱动芯片来做,只是TI没有这么低电压的设计,同时精度0.01mV应该是难以做到的,毕竟开关电源,电压纹波都是10mV以上。