This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27614: 能提供精度0.01mV的可调电压吗?

Part Number: UCC27614


需要选用一款PWM控制器配合C2000控制器给pmos供电。

要求:输出电压在0.12-0.3 V间可调,调节精度为0.01 mV。

请问UCC27614能满足上述要求吗?如果不能,可以推荐几款吗?

谢谢。