This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS563201: TPS563201DDCR 5V输入 2.9A输出 出现限流问题

Part Number: TPS563201

您好:我们正在使用TPS563201DDCR,出现一个问题;
1)IC使用12V输入,3.3V输出;负载仪在2.9A时,其电压输出和负载仪电流正常;
2)但在IC使用5V输入,3.3V输出,负载仪在2.9A时,IC输出电压被拉低到0.3V-0.4V,负载仪电流也被下拉到2.2A左右(明显被限流了,我们使用的外部电源最大电流可达到5A,排除外设试验设备问题)。在将负载仪电流降低到2.5A时,其IC输出正常;我更换过VBST电容由1uf 更换到0.1uF,不良现象依旧。
经过实际计算,上述两种测试条件,外部电源功率一样的情况下(12V输入时,外部供电电源功率为:12.84W;5V输入时,外部供电电源功率为:12.85W),为什么会存在一种输出正常,一种不正常输出现象(不正常的时候,可听到电感的“滋滋”叫声)? 下图为我们的原理设计,还请帮忙分析一下,我们的需求是IC使用5V输入,3.3V输出,输出电流达到2.9A以上,但不会超过3A的最大电流条件;