Part Number: TPS65217
The total power consumption of external load is 350mA@3.3V. Can LDO3 and LDO4 be output in parallel?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS65217
The total power consumption of external load is 350mA@3.3V. Can LDO3 and LDO4 be output in parallel?

LDO内部的工作逻辑是什么? 是检测到过流就关断输出?还是检测到欠压再关断? 我并未从技术规格书上找到相应的说明。
大部分时间,电流还是小于200mA的,但在后端负载全部运营的极限情况下有350mA,我需要能瞬间提供输出,不至于直接关断输出。
理论上:
并联是存在均流问题,但如果内部是欠压保护的逻辑,且一旦有一路到200mA后,输出电压降低的话,电流就会从另一路走。所以持续的200mA是否会对器件造成损伤?
Hi
你可以看一下专门的LDO芯片datasheet,了解其工作原理,尽管datasheet上没有提出不能并联使用,但是LDO却不具备均流能力。
Hi
那还能推荐一款 和TPS65217B 内部LDO结构相同的 LDO芯片吗? 我去查查datasheet。
Hi
只要是LDO应该都是一样的(TPS65217并没有给出LDO的内部结构, 但是TI的LDO结构应该都是一样的)