设计一个仪器,有地板想控制板供电,5V输入给TPS73233,1脚和3脚接输入,2脚接地,4脚悬空,5脚输出,但是无法输出3.3V,买了十片都测试过了,要么输入等于输出,要么值就不对,是在不知道是那部分电路出现问题能产生这样的结果,求教了!!!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
设计一个仪器,有地板想控制板供电,5V输入给TPS73233,1脚和3脚接输入,2脚接地,4脚悬空,5脚输出,但是无法输出3.3V,买了十片都测试过了,要么输入等于输出,要么值就不对,是在不知道是那部分电路出现问题能产生这样的结果,求教了!!!!!
输出电容也拆掉了?LDO电路很简单,不正常多数是输出电容ESR不满足要求造成的。这款可以在无输出电容下稳定,所以推荐这一测试。
隔离模块空载输出会高到6V吗?这款LDO最大输入就6V,过高可能烧坏。
之前您提到10片都测试过有问题,所以有可能都烧坏了。试试把EN接地看看器件还能否关闭。
也有可能是货源的问题,建议向TI申请样片再测试。
麻烦再问一下,空载无电容的情况下,输出应该是多少伏,3.3V稳定输出么?开芯片说明里写的可调节输出是怎么回事,怎么调节啊,还有,在什么情况下能造成这个芯片无法稳定输出3.3V,输入等于输出的时候,是不是就烧坏了,TPS73233对于输入电源有没有什么要求,是不是我的输入电源造成的,我输入电源是一个隔离模块给的,电压在5.2V左右,郁闷中,求救啊,各位大哥大姐们!!!!!
器件末尾33指的是3.3V输出版本。可调版本是01结尾。
无负载无输出电容,TPS73233输出就该是3.3V。
不熟悉隔离模块,它的输出有调制吗?空载下可否用示波器抓一下输出电压。
还得向高人咨询一下,TPS73233想稳住3.3V需要多长时间,是瞬间就能稳到3.3V,还是有个升压和降压的过程啊?大概多长时间啊?求助!!!!!再次拜谢!
Hi
具体的波形你可以查看datasheet: http://www.ti.com.cn/cn/lit/ds/symlink/tps73233.pdf 第十页Figure 23: TURN-ON RESPONSE
不同的负载和输出电容,输出上升到稳压的时间和坡度略有差异,大约都是在500uS左右。