This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP87524-Q1: 最大输出电流

Part Number: LP87524-Q1


您好,

我想要使用LP87524将5V电压转为四个output,电压分别为3.3V,2.7V,1.8V,1.2V。

然后问题在于1.2V这一路的负载电流较大,最大可达到3A,典型1.5A。spec里面写的最大输出电流是4A,但是这个4A的数据并未给出对应的输出电压是什么,所以想具体问一下,如果确定了是输出电压1.2V那一路,那么这一路的最大输出电流是多少?

提前感谢!

祝好

max