Other Parts Discussed in Thread: LMR14206
我使用一片TPS54560将60V降压为12V,然后使用LMR14206将12V降压为5V,接着使用TLV70233降压为3.3V给MCU供电。
将TPS54560的输出作为LMR14206的输入,此时能明显听到LMR14206的电感啸叫。
查看SW波形,发现TPS54560由于功耗过低进入了DCM模式,
此时LMR14206的SW波形很异常、如下图所示。
使用外部独立12V电源作为LMR14206的输入,此时LMR14206电感不啸叫,SW波形也正常。
请问:
这种问题该怎么解决才能让LMR14206电感不啸叫, 对于需要多级电源, 例如60V输入、需要12V、5V、3.3V输出时一般怎么做。