This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952EVM: IIC SCL被拉低

Part Number: BQ76952EVM
Other Parts Discussed in Thread: BQSTUDIO, , BQ76952, EV2400, BQ76940, BQ76930

您好,

我之前购买了一块BQ76952EVM, 可以正常使用BQstudio来评估。但是为了灵活操作测试芯片,我采用了CH341模块,通过IIC控制BQ76952。

在使用IIC的时候,设置频率20K,  BAT电压38V,逻辑分析仪抓取IIC波形如图,其中SCL会被随机性的拉低一段时间,导致信号不能正常传输。

而不接AFE的时候,实际波形如下:

我尝试修改过上拉电阻,外接3.3V上拉电源,但仍然没有效果,希望您这边能够给一些建议,谢谢!