This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610: 无法充电

Part Number: BQ24610


你好!

我现在参考器件datasheet 10.2.1 system with power path 设计的电路,现在接上直流电源作为AC输入,接上电池无法正常充电。具体参数和现象如下:

VIN = 12 V ,I adapter_limit = 3.75A , I charge = 2 A, I pre-charge = I term = 0.3 A,  saltey timer : Disable      电池充电电压 8.4 V

万用表实际测量值如下

ACP = 11.62V                                       VCC =10.9 V

ACDRV =  5.91V                                  BATDRV = 11.62 V

ISET1 = 1 V                                         HIDRV =  7.46 V

ISET2 = 0.75V                                     PH = 7.46 V

ACSET = 0.3 V                                    BTST = 9.28 V

VREF = 3.29 V                                    REGN = 5.99 V

CE = 3.29 V                                         LODRV = 0.12 V

STAT1 = 0.05 V                                   SRP = 7.46 V

STAT2 = 10.06 V                                 SRN = 7.46 V

PG = 0.07 V                                         TTC =  0

TS = 1.66 V                                          VFB = 1.85 V

LODRV 和 PH 的波形如下:

CH1 为 LODRV , CH2 为 PH