This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5041: UVLO和SS引脚掉电时,VREF处电压状态

Part Number: LM5041


LM5041、LM5041A和LM5041B,我看到关于VREF电压的信息是这里

这里的意思是,LM5041B在UVLO引脚掉到欠压值以下的时候,VREF处依然有5V参考值存在。


我想问一下LM5041是否也是这样呢,还是在UVLO引脚低于欠压值的时候,VREF的5V没有了?

或者我将LM5041的SS引脚拉低,VREF是否还有5V参考值存在呢?