This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27211A: UCC27211A

Part Number: UCC27211A

As shown in the figure above, a high-Voltage open-loop BUCK structure is constructed using UCC27211A。

The test conditions: VBUS=50V, VDD=8V,HI,LI fsw=100Khz,D=50%,HI,LI Deadtime=100ns,no Load。

The test wave:

CH1:HS  , CH2:HO, CH3:Inductance current waveform,  CH4:LO

Question:Why does HO fall down in the middle, HS=HO, and the upper tube of the drive is not open???

Please help answer ,thank you very much!