请教一个问题,我在选型时候,发现UC2708N芯片手册中的使用温度写的不一致,手册上半部写的工作温度-25摄氏度,下半部写的工作-40摄氏度,本人比较迷惑,请教是否UC2708N可以满足使用温度为-40。或者不同年份产的该芯片是否使用温度存在不一致的情况。详细请参照图片

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
commercial operation over a 0°C to 70°C temperature range and industrial temperature range of –25°C to 85°C respectively.
所以正确范围–25°C to 85°C.