This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5060: LM5060 接负载后,MOS管短路,是sens pin,out pin击穿短路导致的吗?

Part Number: LM5060


1、最近使用LM5060设计,电压输入是36V~58V,MOS管并联了四个,型号:IPT015N10N5,VDS=100V,ID=300A,引脚9(out pin)目前串接一个0R电阻,EN引脚使用物理按键接通50V来EN,SENSE引脚接9.09K电阻。
2、控制逻辑:接通按键,EN使能LM5060,输出36V~58V电压,关闭物理按键,无使能(EN)LM5060,无输出电压;
3、在有输出电压的情况下,输出负载接了四个电机,在运行一段时间后,按下物理按键,无法关闭LM5060,发现其中一个或两个MOS管已经短路了。
4、咨询:是因为电机的反电动势造成的反向输入电流导致MOS管损坏的吗,还是sens pin,out pin的电阻设置不合理导致?
5、请教:如何解决这个MOS管短路问题。
file:///C:/Users/yangwangxuan/Pictures/%E5%BE%AE%E4%BF%A1%E5%9B%BE%E7%89%87_20220415145541.png