This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ20Z65电流检测电阻设置遇到问题



先使用BQEasy软件进行串并联数、电池容量等基本配置,并设置电流检测电阻为5mΩ(默认值为10mΩ),设置完毕后刷新SBS界面,结果Full Charge Capacity仅为设计容量的一半,觉得不太对劲,又再Pro界面里读出0X71(电流检测电阻)的值为2710(10mΩ),这并不是我设置的5mΩ,请问这是什么情况?我再将1388(5mΩ)的值写入0X71地址,读取出0X71值确认已改为5mΩ,重新刷新SBS,FCC值仍然约为设计容量的一半。  

注意:BQEasy曾经提示过AFE最小的OV阈值为0.05V,如果过流值设置偏小则无效,我已经将AFE的放电过流设置到20A,短路47A,充电短路47A,重试过但是依然不能设置成5mΩ。

请协助解决,谢谢。